//\///// //\ overLIB Hide Form Plugin //\ //\ Uses an iframe shim to mask system controls for IE v5.5 or higher as suggested in //\ http://dotnetjunkies.com/weblog/jking/posts/488.aspx //\ This file requires overLIB 4.10 or later. //\ //\ overLIB 4.05 - You may not remove or change this notice. //\ Copyright Erik Bosrup 1998-2004. All rights reserved. //\ Contributors are listed on the homepage. //\ See http://www.bosrup.com/web/overlib/ for details. // $Revision: 1.1.1.1 $ $Date: 2006/04/27 18:52:55 $ //\///// //\mini if (typeof olInfo == 'undefined' || typeof olInfo.meets == 'undefined' || !olInfo.meets(4.10)) alert('overLIB 4.10 or later is required for the HideForm Plugin.'); else { // Function which generates the popup with an IFRAME shim function generatePopUp(content) { if(!olIe4||olOp||!olIe55||(typeof o3_shadow != 'undefined' && o3_shadow)||(typeof o3_bubble != 'undefined' && o3_bubble)) return; var wd,ht,txt, zIdx = 0; wd = parseInt(o3_width); ht = over.offsetHeight; txt = backDropSource(wd,ht,zIdx++); txt += '
' + content + '
'; layerWrite(txt); } // Code for the IFRAME which is used in other places function backDropSource(width, height, Z) { return ''; } // Hides SELECT boxes that will be under the popup // Checking Gecko version number to try to include other browsers based on the Gecko engine function hideSelectBox() { if(olNs4 || olOp || olIe55) return; var px, py, pw, ph, sx, sw, sy, sh, selEl, v; if(olIe4) v = 0; else { v = navigator.userAgent.match(/Gecko\/(\d{8})/i); if(!v) return; // return if no string match v = parseInt(v[1]); } if (v < 20030624) { // versions less than June 24, 2003 were earlier Netscape browsers px = parseInt(over.style.left); py = parseInt(over.style.top); pw = o3_width; ph = (o3_aboveheight ? parseInt(o3_aboveheight) : over.offsetHeight); selEl = (olIe4) ? o3_frame.document.all.tags("SELECT") : o3_frame.document.getElementsByTagName("SELECT"); for (var i=0; i (sx+sw) || (py+ph) < sy || py > (sy+sh)) continue; selEl[i].isHidden = 1; selEl[i].style.visibility = 'hidden'; } } } // Shows previously hidden SELECT Boxes function showSelectBox() { if(olNs4 || olOp || olIe55) return; var selEl, v; if(olIe4) v = 0; else { v = navigator.userAgent.match(/Gecko\/(\d{8})/i); if(!v) return; v = parseInt(v[1]); } if(v < 20030624) { selEl = (olIe4) ? o3_frame.document.all.tags("SELECT") : o3_frame.document.getElementsByTagName("SELECT"); for (var i=0; i\n\n'); } f = capExtent.onmousemove.toString().match(/function[ ]+(\w*)\(/); if (f&&f[1] != 'anonymous') capExtent.onmousemove = olMouseMove; } //////// // PLUGIN REGISTRATIONS //////// registerHook("createPopup",generatePopUp,FAFTER); registerHook("hideObject",showSelectBox,FAFTER); olHideForm=1; }