Liquid Cooling

As the demands on data centers continue to escalate, the temperatures within these facilities have reached unprecedented levels. To address this challenge, liquid cooling systems have emerged as a cutting-edge solution.

Liquid cooling systems use a non-conductive liquid to cool electronic equipment, like mineral oil or dielectric fluid. The liquid is usually stored in a tank or other containment system.

Through our investment in TMGcore, an award-winning provider of single- and two-phase liquid immersion cooling technology, we can offer solutions for the next generation of high-performance computing technology.

Airdale datacentrre_High Density Compute_3_HiRes_noBG2
1MW PROTO V2 - ISO 3.26

400kW – 2MW+ Liquid-Liquid Heat Exchanger for Liquid Cooled & Hybrid Data Center Architectures

  • Up to 2MW+ Capacity
  • N+1 pumps, drives and filters
  • Extra large filter bodies to maximize filtration area
  • Front access to control panel, VSDs, expansion tanks and filters

Edgebox

Our Edgebox range sets the industry’s standard for the most compact, high density, low Power Usage Efficiency (PUE) data center infrastructure, and are ideal immersion ready servers to solve every high-performance computing (HPC) technology problem.

Edgebox Branded 3

EdgeBox 10

  • Thermal Load: 10kW (18 kW with appropriate heat rejection)
  • Compact: 5.6 sq. ft.
  • Energy Efficient: Partial PUE of 1.03
  • Servers: 8RU of high-density Enterprise class OEM servers
  • Noise Level: Less than 60 dB, effectively silent
  • Power: Flexible and redundant power architecture

What does “Single-Phase” and “Two-Phase” mean?

The terms “single-phase” and “two-phase” in the context of liquid cooling gain their respective names as a result of what happens to the cooling liquid throughout the cooling cycle.

In single-phase cooling systems, servers are vertically installed in a coolant bath containing circulating hydrocarbon dielectric fluid, similar to mineral oil. This fluid makes direct contact with the server components, facilitating effective heat transfer. It remains in a liquid state and is cooled in a cooling distribution unit (CDU) through a heat exchanger. The heated coolant exits the rack via the top, passes through the heat exchanger, and returns with the help of a coolant pump in the CDU.

Two-phase cooling systems follow a similar process but involve servers sealed in an engineered fluorocarbon-based liquid. Unlike single-phase systems, this fluid can undergo boiling even before reaching 50°C. The heat generated by the servers causes the surrounding fluid to boil, changing its state from liquid to gas. The resulting vapor is then condensed back into a liquid by water-cooled condenser coils located at the top of racks. Once the vapor has transformed into a chilled liquid, it re-enters the cycle, where the heat generated by the servers will turn it back into vapor once again.

As liquid cooling systems gain popularity in data centers and other large-scale operations, there are still misconceptions circulating about them.

Articles

Advanced liquid cooling system

Understanding Coolant Distribution Units (CDUs) for Liquid Cooling Efficiency

Learn more about CDUs and how integrating our CDU into your liquid cooling strategy ensures the best thermal management and a solution that adapts to the future of high-density computing.

Videos

Market Overview

Richard Burcher, Product Manager – Liquid Cooling, offers a brief overview of the current market trends.

Chip Densities

Delve into the rise in chip densities and their potential impact on data center operations.

Hybrid Data Centers

Explore the hybrid approach and gain insights on why this could be the future of data center cooling.

Technique Overview

This video outlines the two primary techniques used in liquid cooling.

Technical Comparison

This video explores liquid cooling techniques and highlights some of the pros and cons of different methods.

Heat Reuse

In this video, Richard Burcher examines what heat reuse means for data centers.

Cooling Fluids

This video examines the types of fluids used in liquid cooling and their applications in modern data centers.

The owner of this website has made a commitment to accessibility and inclusion, please report any problems that you encounter using the contact form on this website. This site uses the WP ADA Compliance Check plugin to enhance accessibility.