Airedale by Modine Releases High Capacity Turbocor® Chiller for Data Center Industry

Airedale by Modine release TurboChillTM DCS to deliver improved cooling capacity in higher ambient temperatures for colocation & hyperscale data centers.
Critical Cooling Specialist Airedale by ModineTM has today announced the 2MW TurboChillTM DCS, the next generation in their range of Turbocor® compressor chillers, redesigned from the ground up to meet the specific operational demands of colocation and hyperscale data centers. TurboChill DCS will be manufactured in the U.K. and the U.S. for global distribution.
TurboChill DCS is the latest in Airedale’s DCS range of data center specific chillers, designed to meet the most ambitious efficiency, performance and sustainability objectives. It is optimized for higher ambient temperatures of up to 55°C/131°F, with low GWP refrigerant R1234ze (GWP 1.37). Turbocor® oil-free centrifugal compressors deliver outstanding efficiency across full and part load, and the modular ‘V’ frame coil arrangement has been further optimized with the application of Airedale’s Enhanced Free CoolingTM technology, using larger diameter fans for reduced energy consumption.
An improved water system delivers increased opportunity for free cooling, with the on-board variable speed pump enabling variable primary flow rate control, reducing energy consumption. The enclosed glycol loop separates the glycol from the indoor systems, offering protection from freezing weather conditions whilst ensuring the continued performance of indoor units. Featuring an ultra-low-lift operation, for when waterside free cooling isn’t the right option, the compressors ensure low power consumption in decreasing ambient temperatures. It also delivers lower sound levels for environmental comfort.
Patrick Cotton, Product Management Director for Airedale by Modine said,
“TurboChill DCS is the latest innovation resulting from 20 years’ of Turbocor® compressor experience, combined with 50 plus years data center expertise, to deliver a sustainable, high capacity chiller for colocation and hyperscale data centers.
Patrick continued,
“The market has seen an increased demand for emerging digital technologies, and TurboChill DCS has been developed for easy integration into air or hybrid cooling systems.”
As with all Airedale by Modine chillers, TurboChill DCS comes with the latest helix™ intelligent controls platform inbuilt, and can be integrated into BMS and intelligent optimization cooling systems.
For more information about TurboChill DCS, please visit our TurboChill DCS product page.
Ends
About Modine
For more than 100 years, Modine has solved the toughest thermal management challenges for mission-critical applications. Our purpose of Engineering a Cleaner, Healthier World™ means we are always evolving our portfolio of technologies to provide the latest heating, cooling, and ventilation solutions. Through the hard work of more than 11,000 employees worldwide, our Climate Solutions and Performance Technologies segments advance our purpose with systems that improve air quality, reduce energy and water consumption, lower harmful emissions, enable cleaner running vehicles, and use environmentally friendly refrigerants. Modine is a global company headquartered in Racine, Wisconsin (U.S.), with operations in North America, South America, Europe, and Asia. For more information about Modine, visit modine.com.
Media Contacts:
UK: Nicola Ware | E: [email protected] | Tel: +44 113 2391000
US: Kimberly Raduenz | E: [email protected] | Tel: +1 262-636-1504