Edge Data Center Cooling
We are now living on a planet that runs on data. Connectivity underpins everything we do and the data centre industry is constantly evolving to keep up with not only demand, but also its environmental responsibilities. …
SCC Fareham Data Center
Airedale IQity framework used in SCC Fareham data centre to improve sustainability and efficiency in data centre cooling. …
Data Center Resources
We are now living on a planet that runs on data. Connectivity underpins everything we do and the data centre industry is constantly evolving to keep up with not only demand, but also its environmental responsibilities. …
University of Portsmouth Data Center
Working in conjunction with Sudlows, Airedale was selected for its ability to offer a complete solution encompassing British manufactured, high performance systems, advanced controls and expertise in integrating to third party systems, commissioning and ongoing service and support. …
EMIS data center
EMIS required a new 24/7 data centre as expansion to the existing facility in order to increase its secure and resilient capacity as it extends its range of services to GPs. The data centre incorporates a highly efficient, reliable cooling and monitoring solution designed by Airedale. …
Custodian Data Centres
Working in direct partnership, Airedale designed and built an intelligent, energy efficient data centre cooling solution that significantly reduces the need for mechanical cooling and provides fresh air free cooling up to 80% of the year. …
London Data Exchange
London Data Exchange (LDeX) provides purpose-built, enterprise-grade, network-independent, colocation space and high quality data centre solutions designed to deliver total confidence. …
ClassMate® Unit Ventilator
AireWall™ is a new and innovative low energy cooling solution for mission-critical environments. This range of computer room air handlers (CRAHs) has been specially designed for low velocity air cooling in solid floor, high-density data centre applications with hot-aisle containment. …
DCS Engineering Team
We are now living on a planet that runs on data. Connectivity underpins everything we do and the data center industry is constantly evolving to keep up with not only demand, but also its environmental responsibilities. …