Tower of London
As part of a major refurbishment programme to the Tower of London, Airedale was selected to supply two Ultima™ twin circuit compact chillers to deliver comfort cooling to the building. …
Harrogate International Centre
Avoiding any interruption to normal business operation, HIC management wished to replace two ozone-depleting, potentially hazardous R11 chillers installed when the HIC was opened in the early 1980s, with a more efficient system that would provide a reliable, comfortable environment for audiences, delegates and visitors alike. …
Yorkshire Building Society
Spread over four floors, the 3,200 m2 of operational space in this sealed building is now fully utilised, with people and computers creating a high heat gain. In this business critical application, calls are constantly received from branches, investors and borrowers twelve hours a day, six days a week. …
TRW Automotive
Precision of the end-product is crucial and the intricate, detailed processes demand accurately controlled temperature and humidity. Air quality is also a major priority as all components and equipment must be free from dust and debris from the air. …
Harrogate Hydro
Harrogate Council have support from qualified Airedale technicians whether it be over the phone, on the help desk or, should the need arise, calling an engineer out on site. …